Figure 1: How companies prioritise their technology investments (from forrester consulting thought leadership paper, ‘seamless connectivity fuels industrial innovation’, commissioned by analog devices
Among other points, it is interesting to note that, for medium and high maturity companies, wired connectivity has slightly higher importance than 5G and wireless. However, the key point is that, overall, wired connectivity is one of the critical issues for such companies – but how is this being implemented, and how will it change in the future?
Simon Seereiner, Head of Product Management SAI & IE at Weidmüller, explains: We now use IP-based communication pretty much everywhere - in smartphones and on our computers but also in industrial facilities. Over the last 20 years, we have seen more and more Ethernet-based communication architectures being implemented in industrial applications, such as Profinet, Ethernet IP and Ethercat .
All of these are Ethernet-based field-bus systems. However, there is a lack of consistency right at the last hurdle, i.e., at sensor-actuator level. At this level, we are still using bus architectures such as Profibus, CAN and ASI. This issue grows with an enterprise’s IoT-based, Industry 4.0 infrastructure, which involves dense data volumes being generated by each sensor on every machine or equipment item on the factory floor; this calls for multiple gateways to convert to Ethernet-based communication.
By contrast, today's approach is to establish consistent connectivity so that IP-based communication can be implemented even at the very lowest sensor-actuator level. This brings the promise of a simplified, unified network solution covering the entire factory infrastructure; a concept not previously possible with standard Ethernet-based networks which were too expensive and complicated to use in this context. However, it is now being achieved with an increasingly popular version of Ethernet networking, called Single Pair Ethernet (SPE). While driven by the automotive industry, SPE is equally useful in factory automation – replacing analogue sensors or industrial bus systems, especially if they are multi-protocol.
SPE has been around for 10 – 12 years or so, but engineers are now becoming aware of its advantages over conventional Ethernet, which requires at least two wire pairs at 100 Mb, and four wire pairs for Gigabit cables. With SPE technology, only one pair of wires is needed for the same transfer rates, meaning that only a quarter of the amount of copper is required, as well as only a quarter of the processing time. This not only saves space, but also a huge amount of installation effort and money.
A further key benefit is that the single-pair SPE cable can transfer power as well as data. This is based on a technology called Power over Data Line (PoDL), which allows delivery of up to 60 W to an interface during simultaneous data transmission (100 Mbit), over distances of up to 1000 m. Sensor systems, for example, can therefore be supplied with just one single two-wire cable. As a result, such systems can be easily and cheaply set up in industrial applications with a high density, which in turn helps to increase levels of automation and networking while also implementing processes with an ever-increasing degree of automation.
A closer look at SPE benefits
We have seen from the above that SPE can be a single-technology, IP-based replacement for older systems based on sensors and actuators connected to an industrial Ethernet system via fieldbus links. Here are some ways in which SPE overcomes the challenges of the more traditional approach :
The first advantage to a single twisted pair is more reliable mechanical connectors. Instead of needing eight different conductors to carry signals, only two conductors are used, and only two physical contacts are required for the system to work. This also allows the use of more robust connectors that require stronger mechanical links, such as Mx connectors which can provide environmentally sealed connections.
The second advantage is the significant decrease in cable size. This allows for an increase in cable density when routing networks, thus allowing for more devices to be connected simultaneously (as a result of laying more cable in the same cable ducts). Reduced cable size also reduces the weight of the cable, meaning easier installation when compared to thicker, heavier cables. This also makes it easier for operators to adjust the network as the cable is easier to move and manipulate.
Next there is cost; reducing the number of conductors in a cable reduces its price. Cheaper cables allow for lower-cost installations, which incentivise industrial facilities to upgrade their networks.
Since a cable cannot become simpler than a single-twisted-pair, such a cable installation will most likely be compatible with future changes to the network.
The fourth advantage is simplified mechanical connectivity. While such a cable can be fitted with strong, dedicated connectors, the use of just two wires allows for a designer to choose any connection type they want with ease. If, for example, a sensor system that requires power and a network connection were incredibly small, then an installer could connect a twisted pair using directly soldered connections. Failing that, terminal blocks can be implemented with ease. An installer could also use a cable crimping system to attach their own custom connector that fits with the hardware in question.
SPE standardisation
Ethernet is defined by a number of IEEE 802.3 standards; a subset of these defines the SPE options. These are IEEE 802.3 1000Base-T1, IEEE 802.3 100Base-T1 and IEEE 802.3 10Base-T1. The standards use a single twisted pair cable, Unshielded Twisted Single Pair (UTSP), Category 6A, with differential signals transmitted in full duplex .
Signals between two SPE electronic control units are transmitted simultaneously in both directions. They overlap and run in opposite directions on the SPE cable. Since the respective transceivers know their transmit signals, they can filter out the receive signals.
The 1000Base-T1 interface is based on BroadR-Reach and has been standardised as Single-Pair Ethernet (SPE) by the IEEE working group 802.3bp. 1000Base-T1 corresponds in its technical values to classic Ethernet. Thus, the frame format and the minimum and maximum frame lengths are retained. The error rate is 10−1010-10 and the data rate is 1 Gbit/s. The standard can work with autonegotiation and bridge distances of up to 15 m (1000Base-T1A) or 45 m (1000Base-T1B), as found in buses and trucks. As a modulation method, 1000Base-T1 uses the multivalued pulse amplitude modulation PAM3.
The IEEE working group 802.3bu has standardised a procedure for 1000Base-T1 for the transmission of supply voltages via the STP cable under the designation Power over Data Lines( PoDL).
ISO/IEC JTC1 SC25 WG3 defines the cabling required for the standard, and in turn relies on component standards for cables and connectors created in IEC standardisation groups. Several standards have already been published as part of the introduction of SPE.
IEEE 802.3bp 1000 BASE-T1 "Physical Layer Specifications and Management Parameters for 1 Gb/s Operation over a Single Twisted-Pair Copper Cable" defines single-pair transmission by way of a 15 m UTP channel (type A, unshielded) and a 40 m STP channel (type B, shielded). Both channels are specified for a bandwidth of 600 MHz, may include up to four connectors, and guarantee a transmission capacity of 1 Gbit/s.
The large-scale deployment and successful marketing of SPE depends on full compatibility between all devices, cables and connectors. Two connector faces have managed to win through in the international standardisation selection:
- The connector face as per IEC 63171-1 for wiring premises: This is based on a suggestion by CommScope and known under the synonym variant 1 (LC style) for M1I1C1E1 environments.
- The connector face as per IEC 61076-3-125 is recommended for industry and industry-related applications: This is based on a suggestion by Harting , specifically designed for use in environmental conditions up to M3I3C3E3, and known as variant 2 (industrial style)
MICE describes environmental conditions for installations and provides planners and users with valuable advice for the specification of technical equipment and cabling systems. This involves a description of requirements for their mechanical robustness (M), IPxx degree (I), chemical and climatic resistance (C), and electromagnetic safety (E). In the broadest sense, M1I1C1E1 describes the kind of environment found in an office building, for example, and M3I3C3E3 a rather extreme environment that can potentially occur in industry or outdoors.
Based on the connector face defined in the standard, Harting is preparing a comprehensive product portfolio for industry. Prototypes of this connector face were first introduced around two years ago at the SPS 2016 exhibition, along with the two further connectors ix Industrial and M8 d-coded. Following the standardisation of the Harting ix Industrial, this is now the second connector to become an industry standard.